What is Energy Monitoring device (EMD) ENMOD3P?
Energy monitoring device (ENMOD3P) is a 3 phase / 3 Channel communication energy monitoring device. It is able to monitor circuit up to 100A.
With its ability to wirelessly connect to Wi-Fi, it enables convenient circuit monitoring.
The performance category is Class 2.
You can mount ENMOD3P on the DIN rail along with protection device in the distribution board.
The key features of ENMOD3P are:
It accurately measures real-time values of:
- Voltage
- Current
- Power factor
- Active power
- Apparent power
- Reactive power
- Active energy
- Apparent energy
- Reactive energy
Through the Wiser application for iOS and Android, ENMOD3P provides:
- Support for data availability.
- Overall Energy Management
- Load Monitoring
You can use these features to access and monitor the data for the connected circuits.