What is the minimum pull-out force that the terminals of ZBE1015 and ZBE1025 must withstand when using a 1.5 mm² section wire?
The terminals of ZBE1015 and ZBE1025 must withstand a minimum pull-out force of 40 Newtons (N) when connected with a 1.5 mm² section wire. This requirement is in accordance with the following international standards:
- IEC 60947-7-1
- IEC 60947-5-1
- IEC 60999-1
This specification has been successfully validated during product testing, ensuring compliance and reliability in industrial applications.