The ATS01 features a total of 3 potentiometers, each with specific functions:
Starting Time Potentiometer: This allows you to set the starting time between 1 to 10 seconds. The settings are:
A: 0.5 seconds
B: 2.5 seconds
C: 5 seconds
D: 7.5 seconds
E: 10 seconds
Stopping Time Potentiometer: This enables you to set the stopping time between 1 to 10 seconds. The settings are the same as the starting time:
A: 0.5 seconds
B: 2.5 seconds
C: 5 seconds
D: 7.5 seconds
E: 10 seconds
Initial Voltage Potentiometer: This potentiometer sets the initial voltage applied to the motor when starting, ranging from 30% to 80%. The settings are:
A: 30%
B: 45%
C: 60%
D: 75%
E: 90%