How can we help you today?

Power Monitoring Expert (PME 2024) Vista app shows .”” Subscription watchdog caught 'Real Time Data Proxy did not respond on time. ''Restart 'Vista.___'. ””

Issue : The following error occurs in Vista the live data not shows but the same data also not shows on PME Web App

Image-1

Image-2

Operation timed out. The ION Site Server service on the target machine might have been shut down. "Real Time Data Proxy did not respond on time “ The value has not been read in 11 seconds

Product Line: Power Monitoring Expert (PME 2024)

Cause:
The Windows User not added in WebHMI and Real-Time Endpoints settings and do not marking  as Trusted :

Environment:
PME 2024
Vista Applications

Web Application

Resolution:

Follow the below given steps :

§Select Trust to change the Status to Trusted. The Trusted Date is captured when the status is changed to Trusted.
§ Select Save to apply the changes.
Image-3
§

Schneider Electric India

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings