Understanding and interpreting the Trip Curve MTZ Active MicroLogic 5.0 / 6.0
1. What does this curve represent?
This graph shows when the circuit breaker will trip based on:
- Current (X-axis) → How much current is flowing. It shows current as a multiple of:
- Ir (long-time setting) on left graph
- In (nominal current) on right graph
- Time (Y-axis) → How long the breaker takes to trip. It shows trip time in seconds (log scale)
Top = slow trip (seconds to hours)
Bottom = fast trip (milliseconds)
2. What are the different protection zones?
The curve has three main protection regions:
A. Long-Time Protection (Overload)
Purpose: Protects against overload conditions
Settings:
- Ir = 0.4 to 1 × In
- tr = 0.5 to 30 seconds (0.5 for bottom curve and 30 for top side curve)
Behaviour:
- Small overload → trips slowly
- Bigger overload → trips faster
B. Short-Time Protection
- Range, Isd: Medium faults (~1.5 to 10 × Ir)
Purpose:
- Handles short-circuit currents with delay
- Allows coordination with downstream breakers
Also, Short-Time Protection Can be:
- I²t ON → curve follows energy (I²t) as inverse time (Trip time decreases as current increases, i.e., faster tripping for higher current. Better for thermal protection and coordination
- I²t OFF → fixed delay regardless of fault level
C. Instantaneous Protection
- Range, Ii = 2 to 15 × In (optional OFF)
Purpose:
- Trips immediately for severe faults
Behaviour:
- Almost no intentional delay
- Protects against high short-circuit currents
3. Why are there multiple overlapping curves?
Each band represents:
- Tolerance of breaker operation
- Different adjustable settings
Real breaker trips within this band, not exactly one line.
4.Why the curve “breaks” in between transition between different protection functions
The curve is not a single continuous function — it is a combination of multiple protections:
| Zone | Protection Type | Behaviour |
| Top-left | Long-time (overload) | Thermal, slow |
| Middle | Short-time | Delay / selective |
| Bottom | Instantaneous | Very fast |
“The curve is intentionally segmented because each part represents a different protection function (overload, short-time, instantaneous). The ‘breaks’ occur where control shifts from one protection logic to another, each having a different operating principle.”
5. How to use this curve practically?
In reference to the below graph,
Overload: If current = 5×Ir and tr set at 30s, refer yellow lines:
- Move vertically from 5 on X-axis
- Intersect long-time curve of tr=30s
- Move left → read time
Result: Breaker trips in around 35-40 s
Short circuit: If current = 10×Ir and tr set at .8s with I²t ON, refer magenta lines:
- Move vertically from 10 on X-axis
- Intersect short-time curve tr=.8s
- Move left → read time
Result: Breaker trips in around .6-.8s
Instantaneous: If current = 10×In, refer orange lines:
- Move vertically from 10 on X-axis
- Intersect inst. curve
- Move left → read time
Result: Breaker trips in around .02-.05 s