How can we help you today?

Material Safety Data Sheet ( MSDS ) For VW3A1111

Answer :

In VW3A1111 model, This battery is a lithium coin cell type (CR2032) and is used to power the real-time clock (RTC) during power interruptions.

Data sheet is attached for the same, Also the only available certificates for VW3A1111 are those that meet the defined IEC standards. Please refer to the link below for a comprehensive list of available certificates, along with the specific IEC standards they cover. Please refer below mentioned link for the same.

VW3A1111 Data Sheet

And as per concern of MSDS please refer this link.

VW3A1111 MSDS Certificate

Schneider Electric India

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings