How can we help you today?

Battery details Installed in the TM172PDG42R Controller

Issue : Type of battery installed in the controller . With capacity and technical details .

Product – TM172

Solution:

The battery is a standard Lithium battery BR2032 3V 200mAh.

The Modicon M172 Logic Controller features a battery compartment located behind the removable service door/flap on the lower-left side of the front panel.

ss_ref

Product Line: TM172

Environment:
Web Applications
Diagrams

Schneider Electric India

Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings