How can we help you today?

After applying both the primary and secondary licenses in EPO, the Client Machine is not running as expected. The Runtime Manager is automatically shutting down and displaying a software failure message indicating "no license or no key." EPO 2024

Issue : After applying both the primary and secondary licenses in EPO, the client machine is not running as expected. The Runtime Manager is automatically shutting down and displaying a software failure message indicating "no license or no key."

Image-1

Error – “Software Protection Failure .No key found or  no license available from network.”

Product Line: Power Scada Operation (PSO 2024)

Cause: Client System Setup Wizard settings. If the Control Client option is enabled with a full license Client machine.

Environment:
EPO 2024
Runtime Manager  Applications

Power operation

Setup Wizard

Resolution:

Follow the below given steps :

§Open the Power operation Studio application PSO folder
§Select the Projects click on Setup Wizard.

image-2

§After that open the pop-up screen of Computer Setup Wizard.
image-3
§After that select the by default option .
§When Control Setup Role open in Setup Wizard Setting .
image-4
§In Control Setup Role the Control Client should be disabled the Full License

Schneider Electric India
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
  • Help and Contact Centre
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings