The Secondary Server Showing issue. The server cannot run properly as the Alarm Server service keeps stopping intermittently. Due to this, the Runtime is not starting .Redundant PSO 2024 Runtime Manger Issue
Issue : Connection to partner server rejected. Check both servers have the same alarm server configuration and are registered with the same System Management."
Error – “Connection to partner server rejected. Check both servers have the same alarm server configuration and are registered with the same System Management.”
Product Line: Power Scada Operation (PSO 2024)
Cause: Redundant PC IP not defined Setup Wizard settings for the Alarm Server Properties Setup.
Environment:
EPO 2024
Runtime Manager Applications
Power operation
Setup Wizard
Resolution:
Follow the below given steps :