ViewX script error: "Unknown Error 0x80072efd" when opening or running Mimic files after installation.
Issue : ViewX script error: "Unknown Error 0x80072efd" when opening or running Mimic files after installation.
Solution:
The troubleshooting steps performed were as follows:
Opened GS Server Configuration and navigated to System Configuration > WebX.
Verified that:
HTTP was configured to use Port 80.
Allow local connections only was checked.
In the Local Proxy section, verified that:
HTTP Port set to 80.
Unticked the Allow local connections only option.
Restarted the Geo SCADA Server.
After restarting the server and verifying the backup.