Connection with vamp set software with P3 series relay.
Issue: Unable to connect with vamp set software for iid file.
Resolution:
1- Check the relay firmware version
2-IF the FW version is less than v30. 208 the vamp software is supported.
3- Snapshots are attached .
Product Line: P3U30 , P3F30, P3X
Web Applications