How can we help you today?

LV848527 (Electric Motor MCH) can operates on 250VAC continous supply or not

The Rated Voltage of LV848527 ,Electric Motor MCH for MasterPact MTZ2/MTZ3 Drawout Version, is 200 to 240V AC 50/60 HZ.
The MCH (LV848527) has a maximum upper threshold tripping/operating limit of 1.1 Un (1.1 times the nominal maximum of 240V, which equals 264V for short/transient states and not for continuous use.
Customer will not get desired life by using LV848527 in 250V AC continuously, as small voltage fluctuations in 250V AC will result in voltage exceeding maximum upper threshold limit .
For 250 VAC application refer our LV848528, ,Electric Motor MCH for MasterPact MTZ2/MTZ3 Drawout Version, rated 250/277V AC, 50/60 HZ.

Schneider Electric India

Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings