How can we help you today?

Can EasyPact CVS MCCBs be installed in hazardous (Ex)(ATEX) areas of oil and gas plants?

Oil & gas plants often contain hazardous (Ex) areas classified as Zone 0, Zone 1, or Zone 2. EasyPact CVS MCCBs are not explosion-proof devices and do not carry ATEX/IECEx hazardous-area certification. Therefore, they should generally be installed:

  • Inside a safe area electrical room, or
  • Within a suitably certified enclosure/panel located according to the hazardous area classification requirements.

Schneider Electric India

Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings