How can we help you today?

Error 5018 & 5019 in SCADAPack 47XX

Error 5018 & 5019 are known firmware-related issue that can occur on SCADAPack 47x/47Xi devices running RemoteConnect firmware versions earlier than 3.5.5 (Firmware Version 9.13.5). Under certain conditions, the issue can trigger a false status code 5018 or 5019 and cause the controller logic to enter a NOCONF state.

This issue has been resolved in SCADAPack x70 R3.5.5 / Firmware 9.13.5 and later.

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings