On which terminal we can connect ULP Cord for BCIM in MTZ Active ACB?
BCIM Auxiliary supply 24V DC , should be Provided in COM terminal
Supply the ULP module with 24 Vdc SELV (Safety Extra Low Voltage), paying attention to polarity.
The BCIM module is supplied by the power supply of the ULP module.
Two COM terminal block markings are possible:
Terminal E1 (or F2+) is to be connected to 24 Vdc ( Red Color ULP Wire )
Terminal E2 (or F1-) is to be connected to 0 Vdc. (Black Color ULP wire)
Terminal E5 (Blue color ULP wire ) Communication wire
Terminal E6 (White Color ULP wire ) Communication wire .