How can we help you today?

Why energy values are reset to zero in EM6436H meter?

The meter lets you configure any one power parameter (W, VA, or VAR) at a time.
You can set it using the meter’s display, through communication using ION Setup,
or by any Modbus tool that supports FC16 (command number is 2959).


Energy accumulation in the meter depends on the selected power parameter (W,
VA, or VAR). Integrated energy values and old values also depend on the
selected power parameter.

NOTE:
• On changing the power parameter (either through meter display or
communication), all the stored energy values (old and integrated) are
reset to zero.
• Energy values can also be cleared through communication. Run Hours
are displayed with 6 digit Hours and 2 Digit Minutes.

Schneider Electric India

Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings