How to change the WIFI access point for Wiser app (in change to network change)?
To change the device's Wi-Fi Access point:
1. On the Devices page, select the energy monitoring device for which you wish to change the Wi-Fi.
2. In the top-right corner of the screen, tap Settings
3. If Device Status is Online:
a. Tap Change Access Point (B).
A pop-up will appear, asking for the password of the Wiser app.
b. Tap Please enter password, enter the Wiser app password, and Tap Confirm.
c. Select your preferred Wi-Fi network, enter the password in the Wi-Fi Password field and tap Connect.
4. If Device Status is Offline:
a. Tap Change Access Point. A pop-up will appear, asking for the password of the Wiser app.
b. Tap the Please enter password field and enter the Wiser app password, then tap Confirm. This will initiate pairing mode in the Wiser app.
Pairing with a new device will remain the same as when previous devices were added