"Insufficient License Available" Error Despite Valid License in GEOSCADA EXPERT
Issue
When attempting to log in to the Geo SCADA Expert 2023 / ViewX server, the client remains Offline and displays the following message:
Communications Problem
"There are insufficient licenses available for this client."
Solution
Open Windows Services.
Check the status of Geo SCADA Expert License Server.
If the service is stopped, restart the service.
Reopen the ViewX client and log in again.
After ensuring the license server service is running and the client configuration is correctly configured, the client should successfully obtain a license and connect to the server.