Switchgear: Medium voltage explained

Woman girl at factory in a vest and helmet pointing

Protection

Protection

It serves a critical function as the switchgear's primary mechanism for protecting the system against catastrophic failures.

  • Fault detection

    Internal sensors and protective relays constantly monitor current and voltage for sudden surges caused by short circuits or overloads.

  • Rapid interruption

    Upon detection, the relay commands a circuit breaker to open the circuit in milliseconds, isolating the damaged section before the massive energy can cause fire or equipment destruction.

Ringmaster AirSeT

Control

Control

It serves a key management role, enabling human operators and automated systems to manage the flow of electricity.

  • Load switching

    Engineers can close or open specific circuits to connect or disconnect equipment, allowing power to be rerouted during equipment upgrades or maintenance.

  • Monitoring and automation

    Modern MV switchgear is often digitally native, allowing for remote monitoring and control, which improves efficiency and grid resilience (smart grid functionality).

Electrician Engineer and Businessman having meeting in front of switch panel in electrical room at solar cell power plant

Isolation

Isolation

It acts as a critical assurance, helping protect workers during maintenance on critical systems and reducing operational risks.

  • Visible separation

    Using a disconnect switch, also known as an isolator, an air gap is created to separate equipment from live power, ensuring the circuit is fully de-energised for work.

  • Switching devices

    The separation can also be achieved through devices such as a fuse switch disconnector, an earthing switch, or a circuit breaker.

Circuit breaker

Breaks the current flow when a fault occurs and is essential for arc quenching and system protection.

Protective relay

The "brain" that monitors the power and signals the breaker to trip. It determines the precise timing and location of a fault.

Busbar

High-capacity rigid conductors that route power throughout the cabinet, serving as the main electrical pathway.

Instrument transformers

Devices that scale down high voltage and current for measurement, enabling accurate monitoring and protection.

Young engineer
Discover our SF₆-free AirSeT – a sustainable alternative to MV switchgear that often uses SF₆ gas with high GWP.
SF6-free pure air

Find out more about our sustainable SF₆-free MV switchgear technology. Learn why it's worth using.
Two technicians inspect an open electrical panel; one holds a laptop for diagnostics
Explore smart solution that optimise grid applications, improve power quality, cut costs, and boost efficiency.
Medium voltage power distribution - Product Panorama
View the full catalogue and discover the best solution for your facility.

FAQs

Medium voltage typically ranges from 1 kV to 36 kV (IEC) or up to 69/72 kV (ANSI/NEMA), depending on regional standards.​

SF₆ is a gas with a very strong impact on global warming. Because of this, new regulations are beginning to restrict its use in new equipment. The industry is now shifting to alternative options such as pure air, vacuum, or solid insulation materials, which deliver the same performance without harming the environment.

Arc flash, insulation failure, mechanical wear, and improper operation can occur. Proper personal protective equipment, such as protective clothing, helmets, and goggles, along with established procedures, is essential.

Yes. Many modern MV switchgear systems can be monitored and operated remotely using digital tools. This helps detect issues early, plan maintenance, and keep power systems operating smoothly.

Typically, 20 to 30 years, depending on usage, environmental conditions, and maintenance practices.
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings