오늘 무엇을 도와드릴까요?

Can the VW3A28101 HMI be used on the ATV312 drives?

Issue:
Wondering if the VW3A28101 HMI works with the ATV312 drives.

Product Line:
Altivar ATV312

Environment:
All

Cause:
Customer has a spare part keypad VW3A2801 and wants to use it on the ATV312 drive.

Resolution:
No, this HMI will not work on the ATV312 drive.  It only works on the ATV28 drives.