오늘 무엇을 도와드릴까요?

What is a CFF fault on the ATV312 drives?

Issue:
CFF fault causes on the ATV312 drives.

Product Line:
Altivar ATV312

Environment:
All

Cause:
Configuration Fault

Resolution:
Check to see there was an option board removed.
Try resetting the drive back to a factory reset.
ATV312 programming manual BBV46385