ION7550/ION7650 front panel phasor diagram tab values are different than revenue values on other tabs
Goals and Symptoms
Symptoms
-
- The ION7550/7650 meter displays a consistent value for current across the displays but values such as power factor and phase angle can deviate from readings shown on other tabs such as 'Summary2'.
Note: This only applies to meters with the NI Current Probe option.
- The ION7550/7650 meter displays a consistent value for current across the displays but values such as power factor and phase angle can deviate from readings shown on other tabs such as 'Summary2'.
Causes and Fixes
When ordering a non-intrusive (NI) current probe model of the ION7550/7650, some screens such as the phasor diagram tab do not use the calibrated readings of the probes. The phasor diagrams in this model are useful for diagnosing wiring issues, but for accurate readings, such as power factor, the values in the power meter module should be referenced.
Detailed information about what values are affected because of the calibrated current probes and for further information about the NI, NICP, and NICT models of the ION7550 and ION7650, please see https://www.se.com/us/en/download/document/7EN02-0248/
Legacy KB System (APS) Data: RESL208373 V2.0, Originally authored by DaDu on 06/12/2012, Last Edited by MaTh on 06/18/2012
Related ranges: ION7550/ION7650
Product line
PME ION7550 and ION7650