오늘 무엇을 도와드릴까요?

What is the input impedance on the voltage inputs of ION8650?

Issue
What is the input impedance on the voltage inputs of ION86x0?

Product Line
ION8650
ION8600

Environment
Voltage Measurement input impedance specification

Resolution
The AUX power order options of the ION86x0 have no design capacitance on the voltage measurement terminals. On these meters, the measurement terminals have 5 Meg-Ohms to Earth on all four terminals (V1, V2, V3, Vref).
The blade-powered order options do have a capacitive network for EMC filtering. The precise characteristics will depend on which terminals are used for the installation. See attached a simplified schematic diagram.

슈나이더 일렉트릭 Korea

첨부 파일
8650_PSU_capacitor_network.png [25.75 KB]