FAQ 검색
Osisense XC standard - what is the ZCKZ1S06 part number?
The ZCKZ1S06 part number does not appear into the catalogue pages (XCKJ spare parts & accessories). It is an adapted spare parts, created for an OEM in Europe, without any sales limitation. It is in fact the blue front cover without led of the ZCKJ fixed body, which is not sold separately according to the catalogue pages. The specificity "S06" means this blue front cover is equipped with a ventilator to avoid internal condensation into the switch casing. Logistic situation in March 2020: accessory discontinued. Attached corresponding picture. For information, it is used in the ZCKJ1H29S33 adapted contact body, available to order in March 2022
게시 대상:슈나이더 일렉트릭 Korea
첨부 파일
자세히 알아보기