Why can I not set my transient percentage below 105 for my ION 7650 meter?
Issue:
A customer is configuring the transient power quality setting and wants to use a percentage lower than 105.
Product Line:
ION 7650 meters
Environment:
ION Setup
Cause:
This is a restriction that is hard coded into the ION Transient Module.
Resolution:
The lowest value which can be selected is 105% percent and the upper limit is 1000%.