How to add the catch on the fly feature to an ATV630 and ATV930
Product line:
Altivar Process 630 and 930
Cause:
Catch on the fly detects a spinning load and picks up control from that speed. Disabled, the drive will start from zero speed.
Resolution:
The ATV600 and ATV900 series both have a Catch on the Fly option.
ATV600 series: this parameter is enabled by default
ATV900 series: this parameter is disabled by default
Go to Complete Settings > Error/Warning Handling > Catch on the Fly > Catch on the Fly to adjust this parameter.
If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:
Frequently Asked Questions - Schneider Electric (se.com)
If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.
If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)
게시 대상:슈나이더 일렉트릭 Korea