Product Line:
Altivar ATV630/ATV930
Environment:
All
Cause:
Circuit breaker keeps tripping when trying to power up the drive.
Resolution:
The circuit breaker is tripping because it is sensing a short circuit or over current in the circuit. Before repowering the drive you will need to do a full diode check on the inputs and the outputs on the drive.
Do a visual on the drive with no power applied check to see if there are any burn marks on the drive.
Check the breaker settings to see if they may need to be adjusted.
게시 대상:슈나이더 일렉트릭 Korea