오늘 무엇을 도와드릴까요?

Can I use a generic SD card with the HMIG3U HMI?

Issue:
Using a generic SD card with the HMIG3U HMI


Product Line:
HMIG3U, Vijeo Designer


Resolution:
You may use any generic SD memory card up to 32Gig formatted for FAT32. There are different speed class. No particular speed class is required, however the higher the class number the faster the speed. Class 10 is recommended for better performance.