Чем мы можем помочь сегодня?

For Masterpact air circuit breaker (ACB) of type NW or NT, what are the avilable trip unit types and what arethe main protection functions supported by these trip units ?

- For the Masterpact ACB of type NW or NT, the available trip units for these range are of the Micro logic type trip units.

- These Micro logic trip units are found in the following types:

1- Micro logic (2): used for basic protection  which include (Long + Instantaneous) Protection supported.
2- Micro logic (5): used for basic protection  Which include (selective zone feature + Long + Short + Instantaneous) protection supported.
3- Micro logic (6): used for selective protection (same as Micro logic 5) + earth fault protection.
4- Micro logic (7): used for selective protection (same as Micro logic 5) + earth leakage protection.