Issue:
Does the Altivar ATV58 have a Profibus communication option?
Product Line:
ATV58
Environment:
All
Cause:
Profibus option
Resolution:
Yes. The Profibus communications card is part number VW3A58307U. However, it is obsolete and there is no replacement available.
Does the Altivar ATV58 have a Profibus communication option?
Product Line:
ATV58
Environment:
All
Cause:
Profibus option
Resolution:
Yes. The Profibus communications card is part number VW3A58307U. However, it is obsolete and there is no replacement available.
Опубликовано для: Schneider Electric Казахстан