Наши бренды

Impact-Company-Logo-English Black-01-177x54

Добро пожаловать на сайт Schneider Electric

Добро пожаловать на наш сайт.
		
Чем мы можем помочь сегодня?
What is the part number for ATV61 and ATV71 Modbus TCP/IP (Ethernet) option card?
Issue:
ATV61 and ATV71 part number for Modbus TCP/IP option card.

Product Line:
Altivar 61 and Altivar 71

Environment:
All part numbers, all models

Cause:
Customer could not find the part number

Resolution:
The part number of the Dual port (Daisy Chain) TCP/IP Ethernet option card is VW3A3310D.
VW3A3320 is also an option since it will support either ModBus TCP/IP or Ethernet IP.

Be sure to check the firmware version of your drive and confirm it's compatible with the option card.