Наши бренды

Impact-Company-Logo-English Black-01-177x54

Добро пожаловать на сайт Schneider Electric

Добро пожаловать на наш сайт.
		
Чем мы можем помочь сегодня?
How to turn off the input phase loss in an ATV61 when using single phase?
Issue:
ATV61 Phase loss deactivate

Product Line:
All

Environment:
All

Cause:
Supply voltage single phase

Resolution:
To disable Input phase loss
Under the Main Menu
Go to the Drive Menu enter
Go to the Fault Management Menu 1.8  enter
Go to the "Input Phase Loss" parameter enter
Set "Input Phase Loss" to no (off)