Наши бренды

Impact-Company-Logo-English Black-01-177x54

Добро пожаловать на сайт Schneider Electric

Добро пожаловать на наш сайт.
		
Чем мы можем помочь сегодня?
Can't get part number SFD212FG4Y to come up in our system?

Issue:
Can't get part number SFD212FG4Y to come up in our system?

Product Line:
All ATV212 S-Flex enclosures

Environment:
All ATV212 S-Flex enclosures

Cause:
Can't get part number SFD212FG4Y to come up in our system?

Resolution:
Need to add a B07D07 or just a D07 to the end of the part number.  B07-line contactor and D07- keypad.