FDR is supported on the BMXNOE0100 and BMXNOE0110. It is not supported on the BMXP342020 or BMXP342030 CPU.
BMXNOE0110 The FDR service on all VW3A3310 and VW3A3310D (below V3.0 IE06) doesn't work with BMXNOE0100 and BMXNOE0110 Ethernet couplers.
VW3A3310D (Version 3.0 IE06 and above) will work with BMXNOE0100 and BMXNOE0110 Ethernet couplers.
FDR is supported on the M580 CPU modules and not the M580 BMENOC03x1 modules. Due to M580 security, The DHCP and Address Service need to be enabled and configured.
Опубликовано для: Schneider Electric Казахстан