Issue:
Is it possible adjust the nominal current of an ATS48C41Y below 0,4 IcL?
Product Line:
ATS48
Resolution:
It's not possible to modify the soft-starter by replacing the control board because there is an EEPROM inside the power board containing the size ( nominal current, etc... ) and there is an auto-adaptation between both cards. The thermal protection is made with PTC on the heatsink and calculation with the thyristors. The best solution is to replace the ATS to a smaller size.
“If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:
Frequently Asked Questions - Schneider Electric (se.com)
If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.
If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)“
Опубликовано для: Schneider Electric Казахстан