Goals and Symptoms
If you use an array (ex : MyArray : ARRAY[0..9] OF EBOOL) with comments and/or initial values for the elements of the array, at the moment you will resize the array (ex: ARRAY[0..10] OF EBOOL) you will lose all the comments and initial values of the elements.
Causes and Fixes
The workaround is to use DDT array. Define an array in DDT tab of DataEditor, and after create instances of this type. Then if you resize the type you will not lose the comment of the instance.
Legacy KB System (APS) Data: RESL172274 V2.0, Originally authored by on , Last Edited by on
Related ranges: Unity Pro
Опубликовано для: Schneider Electric Казахстан