Чем мы можем помочь сегодня?

How many e-mails can be sent out at one time from the M340 CPU with Unity Pro 4.0?

Issue:

Need to know the maximum number of emails that can be sent simultaneously from an M340 CPU when using Unity Pro 4.0.

Product Line:

Modicon M340 CPU

Unity Pro 4.0

Environment:

Sending emails using the M340 embedded Ethernet port

Cause:

The M340 embedded Ethernet port has a limit on the number of concurrent email transmissions it can handle.

Resolution:

A maximum of 4 e-mails can be sent out simultaneously from the M340’s embedded Ethernet port.