Webgate client file is version specified and provided with the Vijeo Designer disk. It is only needed when the Web Server data location is set to Main Drive.
The Webgate Control file is downloaded directly from the target when the Web Server Data location is set to secondary or Optional.
Опубликовано для: Schneider Electric Казахстан