Issue
Customer has a modem type that is not in the ION enterprise modem database and would like to add a new modem.
Product Line
ION Enterprise
Environment
ION enterprise modem database
Cause
If a customer has a modem type that is not in the ION Enterprise modem database, it is possible to add a new modem
Resolution
To configure custom modem settings:
- Download the nonmodem setup tool from the FTP site
- Visit the modem manufacturer web site to get the AT strings.
- You will need to copy a modem setting (so that USER appears after the modem type) then you can adjust the settings & save. This will then be available in the management console as a selectable modem type.
Опубликовано для: Schneider Electric Казахстан