Issue:
ATS48 circuit fuse or circuit breaker data.
Product Line:
Altistart ATS48
Environment:
ATS48
Cause:
Fuse or Circuit breaker protection for the ATS48 soft starter.
Resolution:
Refer to the ATS48 Installation Manual, which includes this table:
For IEC ratings see the charts starting on page 15 using the page link below or attached document.
https://www.se.com/us/en/download/document/DIA2ED2140604EN/
Опубликовано для: Schneider Electric Казахстан