Issue
User would like to know the minimum current required for CM2000 to measure current
Product
CM2000
Resolution
There must be 25 milliamps on the CT secondary or 0.5% of the CT primary ratio to wake up current readings.
For more information, see detailed datasheet here
Опубликовано для: Schneider Electric Казахстан