Issue
Can the BMXART0814 module be used without the ABE7CPA412 and maintain use of all 8 channels for Thermocouple operation?
Product Line
Modicon M340, Modicon M580, X80 IO.
Resolution
Yes. Using a 2-wire PT100 RTD wired to channel 4 on terminals EX+ and EX-. This will allow all 8 channels of the BMXART0814 to be used for thermocouple operation as configured and with a single CJC from Channel 4. Channel 4 will have the 2-wire RTD on EX+ and EX- and the TC on MS+ and MS-.
Опубликовано для: Schneider Electric Казахстан