Наши бренды

Добро пожаловать на сайт Schneider Electric

Добро пожаловать на наш сайт.
		
Чем мы можем помочь сегодня?
Can you put line reactors on an ATS22, ATS23, ATS46 or ATS48 Altistart Soft starters?

Article available in these languages: Czech

Issue:
Are line reactor required on the Schneider Electric Soft starters?

Product Line:
ATS22, ATS48, ATS46, ATS01, ATS23

Environment:

All

Cause:

Will the Schneider Electric ATS soft starters required any filtering or line conditioning device up stream.

Resolution:
No, the Schneider soft starters do not required any filtering or conditioners up stream.   Soft starters only ramps up the voltage with very little harmonic distortion.