The RA1GA*** are out of production since several years (>10). The RA1GA75105 was a three phase thermal relay for setting between 75 and 105A. You can replace it by a LR9G115 from 28 to 115A or LR9G225 from 57 to 225A.
Опубликовано для: Schneider Electric Казахстан