Issue:
DC Choke availability for ATV61 and ATV71 drives.
Product Line:
ATV61 and ATV71
Environment:
All models and serial numbers
Cause:
None
Resolution:
DC Chokes are not in our offering for spare parts on the Frame sizes 2 thru 8.
DC Chokes are offered as replacement parts only on some of the Frame sizes 9 thru 15.
Contact the Drives Product Support Group for assistance 1-888 778 2733.
Опубликовано для: Schneider Electric Казахстан