Наши бренды

Добро пожаловать на сайт Schneider Electric

Добро пожаловать на наш сайт.
		
Чем мы можем помочь сегодня?
How tall is the NetShelter WX with the optional castor kit attached?
Issue:
Customers may ask for the total height of the NetShelter WX with the optional castor kit attached.

Product Line:
NetShelter WX

Environment:
All versions and serial ranges.

Cause:
Cabinets that are floor mounted may have height restrictions.

Resolution:
The NetShelter WX with the optional castor kit attached is approximately 731 mm (28.78") tall.