Наши бренды

Impact-Company-Logo-English Black-01-177x54

Добро пожаловать на сайт Schneider Electric

Добро пожаловать на наш сайт.
		
Чем мы можем помочь сегодня?
Do the ATS01 soft starts have combination short circuit current ratings?
Issue:
Combination of short circuit current ratings on ATS01

Product Line:
ATS01

Environment:
All Modes and Serial Numbers

Cause:
None

Resolution:
The ATS01 soft starts do not have overload protection so they cannot be used in combination with other components to achieve the combination short circuit current ratings.