Наши бренды

Impact-Company-Logo-English Black-01-177x54

Добро пожаловать на сайт Schneider Electric

Добро пожаловать на наш сайт.
		
Чем мы можем помочь сегодня?
Can the EFB blocks created with the EFB toolkit have extensible output pins?
Issue
Can the EFB blocks created with the EFB toolkit have extensible output pins?

Product Line
EFB toolkit.

Environment
Windows 7, Windows 10, Windows 8

Resolution
No, it is not possible to have extensible output pins on an EFB block created with the EFB Toolkit..