Issue:
Reading the Nominal Current Range of the ATS22 from part number
Product Line:
Altistart ATS22
Environment:
All
Cause:
Needs to be able to tell the soft starters current ratings.
Resolution:
Look at the part number example the ATS22D88 is rated for 88 amps or the ATS22C17 is rated for 170 amps.
Опубликовано для: Schneider Electric Казахстан