Issue:
Shows how to setup plus and minus speed on the ATV212.
Product Line:
ALTIVAR 212
Environment:
All serial number
Cause:
N/A
Resolution:
Follow these steps to program terminal R for plus speed, and RES for minus speed.
Frequency Mode Select (FNOD) = 5 (+/- speeds)
Logic input R (F112) = 41 (+ speed)
Logic input RES (F113) =42 (- speed)
See ATV212 Programming manual for details.
https://www.se.com/ww/en/download/document/S1A53838/
Опубликовано для: Schneider Electric Казахстан